Processor Expert support for M52259DEMOKIT in CodeWarrior for ColdFire V7.2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Processor Expert support for M52259DEMOKIT in CodeWarrior for ColdFire V7.2

1,005 次查看
PeteG
Contributor II

Hi

I'm using CodeWarrior for ColdFire V7.2 with a M52259DEMOKIT.

If I try to use Processor Expert or Device Initialisation I get a message saying that the M52259DEMOKIT is not supported. Is this correct and are there any updates to add this support?

 

I've noticed that the patch for CodeWarrior for ColdFire V7.1.2 adds support for this board but I can't find anything for CodeWarrior for ColdFire V7.2.

 

Thanks

标签 (1)
0 项奖励
回复
1 回复

499 次查看
ProcessorExpert
Senior Contributor III

Hello,

 

we are sorry for inconvenience but currently there are supported only M52259EVB rev 2.0 and plain M52259 MCU in Processor Expert.

 

To use 52259DEMO, you could create a regular project for plain 52259 (not EVB) and setup the CPU bean according to DEMO PCB hardware (crystal etc..).

 

best regards
Vojtech Filip
Processor Expert Support Team

0 项奖励
回复