Problems getting correct remote system on a MC9RS08KA1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problems getting correct remote system on a MC9RS08KA1

715 次查看
barbercolman
Contributor III

When I import a MC9RS08K81 from CW 6.3 the project uses a remote system RS08BDM_PandE_Multilink_CyclonePro. When I launch the debugger it appers to find the part, program the part. However connection is lost when attempting to debug. I have attachec a screen shot what shows the erroror message.

 

When I create a new bearbone project i get a PnE U-MultilinK and it can find the part, program the part and then stop at main. Screen shot attacched.

 

I have tried adding the PnE U-MultilinK to the other project and it does not show up in the new remote connections.

标签 (1)
0 项奖励
回复
1 回复

561 次查看
J2MEJediMaster
Specialist I

Based on what you told me, a bare-boned project, fresh from the New Project wizard, builds and debugs through the run-time probe. The imported project does not connect, or stay connected, with the probe. Would it be possible to just move your source code files to bare-boned project and use that instead?

 

---Tom

0 项奖励
回复