Problems getting correct remote system on a MC9RS08KA1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problems getting correct remote system on a MC9RS08KA1

1,064件の閲覧回数
barbercolman
Contributor III

When I import a MC9RS08K81 from CW 6.3 the project uses a remote system RS08BDM_PandE_Multilink_CyclonePro. When I launch the debugger it appers to find the part, program the part. However connection is lost when attempting to debug. I have attachec a screen shot what shows the erroror message.

 

When I create a new bearbone project i get a PnE U-MultilinK and it can find the part, program the part and then stop at main. Screen shot attacched.

 

I have tried adding the PnE U-MultilinK to the other project and it does not show up in the new remote connections.

ラベル(1)
0 件の賞賛
返信
1 返信

910件の閲覧回数
J2MEJediMaster
Specialist I

Based on what you told me, a bare-boned project, fresh from the New Project wizard, builds and debugs through the run-time probe. The imported project does not connect, or stay connected, with the probe. Would it be possible to just move your source code files to bare-boned project and use that instead?

 

---Tom

0 件の賞賛
返信