Open/Close Projects in Eclipse IDE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Open/Close Projects in Eclipse IDE

3,683 Views
ignisuti
Contributor IV

My options for Opening and Closing a Project in the Eclipse IDE are disabled.

 

Why would this be? I can build code and create new projects.

Labels (1)
0 Kudos
Reply
8 Replies

2,750 Views
J2MEJediMaster
Specialist I

What operating system are you using? What directory did you install CodeWarrior in?

 

---Tom

 

0 Kudos
Reply

2,750 Views
ignisuti
Contributor IV

Windows 7 64-bit version.

 

C:\Program Files (x86)\Freescale\CW MCU v10.1

0 Kudos
Reply

2,750 Views
J2MEJediMaster
Specialist I

Try taking a look at this https://community.freescale.com/message/67170#67170. If that doesn't help, try submitting an on-line service request.

 

---Tom

 

0 Kudos
Reply

2,750 Views
CrasyCat
Specialist III

Hello

 

You can also try to install CodeWarrior outside of the C:\Program Files (x86) folder.

 

Uninstall CodeWarrior and use it for example in C:\Freescale as root directory for the installation.

 

CrasyCat

0 Kudos
Reply

2,750 Views
ignisuti
Contributor IV

Nope. Still no luck.

0 Kudos
Reply

2,750 Views
CrasyCat
Specialist III

Hello

 

Do you have at least one project showing up in your CodeWarrior projects view?

 

If not it is normal that the Open Project and Close Project menu entry are disables.

 

Close Project is used to close an opened project in the CodeWarrior Projects View.

Open Project is used to open a previously closed project in the CodeWarrior Project view.

 

 

 If you want to add an existing project you need to import it into the IDE using File > Import > General > Existing Projects into the workspace.

 

CrasyCat

0 Kudos
Reply

2,750 Views
ignisuti
Contributor IV

I see. I guess this is normal behavior then. I have to actualy click on the Projects Window before Close Projects becomes available..

 

Thanks guys.

0 Kudos
Reply

2,750 Views
CrasyCat
Specialist III

Hello

 

Yes this is normal behavior.

As you can have multiple projects opened simultaneously in the CodeWarrior Projects window, you need to select the project you intend to close before you can select Project > Close Project.

 

CrasyCat

0 Kudos
Reply