Installing Code Warrior 8.7 on Windows 7 (64-bit)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Installing Code Warrior 8.7 on Windows 7 (64-bit)

ソリューションへジャンプ
9,610件の閲覧回数
am304
Contributor I

Hi,

 

I realise this isn't officially supported, but my laptop was recently upgraded to a machine running Windows 7 64-bit. I am trying to install CodeWarrior for PowerPC 5XX v8.7 (using "run as administrator") but the installer eventually errors out saying:

 

"The wizard was interrupted before CodeWarrior Development Studio, MPC5xx Edition, v8.7 could be completely installed.

 

Your system has not been modified. To complete installation at another time, please run setup again"

 

Click Finish to exit the wizard".

 

Has anybody come across this or tried to install Code Warrior for MPC5xx v8.7 on Windows 7? Is there a workaround?

 

Many thanks in advance,

 

Arnaud

ラベル(1)
0 件の賞賛
返信
1 解決策
3,270件の閲覧回数
kef
Specialist I

I'm not sure if Natep's  solution for CW for S12 V5.0 is applicable for CW for PowerPC:

 https://community.freescale.com/thread/57404

 

But the symptoms were the same - "was interrupted" message. Hope it will work also for CW for PowerPC

 

You need to find working 32bits Win XP machine and install CW there. Then:

 

2) Copy whole CW folder from Win32 machine to Win7 machine (Program Files\CodeWarrior xxxx)

3) Now, this step is the MOST IMPORTANT:

    Look at the file "Mwregsvr.exe" in the c:\Program Files(x86)\Freescale\CodeWarrior for Microcontrollers V6.1\bin and click the right button on this file, then click properties.

    Now, in the compatibility tab,set the compatibility to WindowsXp (sp2) and set the checkbox

    to run in administrator mode.

    Now, click apply button then click OK button.

4) In the same folder, run once the file regservers.bat

    When windows ask for the permisions, just click yes everytime.

 

5)  You may want to create a desktop icon at this point.

 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,271件の閲覧回数
kef
Specialist I

I'm not sure if Natep's  solution for CW for S12 V5.0 is applicable for CW for PowerPC:

 https://community.freescale.com/thread/57404

 

But the symptoms were the same - "was interrupted" message. Hope it will work also for CW for PowerPC

 

You need to find working 32bits Win XP machine and install CW there. Then:

 

2) Copy whole CW folder from Win32 machine to Win7 machine (Program Files\CodeWarrior xxxx)

3) Now, this step is the MOST IMPORTANT:

    Look at the file "Mwregsvr.exe" in the c:\Program Files(x86)\Freescale\CodeWarrior for Microcontrollers V6.1\bin and click the right button on this file, then click properties.

    Now, in the compatibility tab,set the compatibility to WindowsXp (sp2) and set the checkbox

    to run in administrator mode.

    Now, click apply button then click OK button.

4) In the same folder, run once the file regservers.bat

    When windows ask for the permisions, just click yes everytime.

 

5)  You may want to create a desktop icon at this point.

 

0 件の賞賛
返信
3,270件の閲覧回数
sbsoccermike
Contributor I

Does anyone know if using SP3 is better or worse than SP2 for this application?

0 件の賞賛
返信
3,270件の閲覧回数
am304
Contributor I

Thanks, that worked a treat!!

 

Arnaud

0 件の賞賛
返信