Installing Code Warrior 8.7 on Windows 7 (64-bit)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Installing Code Warrior 8.7 on Windows 7 (64-bit)

Jump to solution
9,611 Views
am304
Contributor I

Hi,

 

I realise this isn't officially supported, but my laptop was recently upgraded to a machine running Windows 7 64-bit. I am trying to install CodeWarrior for PowerPC 5XX v8.7 (using "run as administrator") but the installer eventually errors out saying:

 

"The wizard was interrupted before CodeWarrior Development Studio, MPC5xx Edition, v8.7 could be completely installed.

 

Your system has not been modified. To complete installation at another time, please run setup again"

 

Click Finish to exit the wizard".

 

Has anybody come across this or tried to install Code Warrior for MPC5xx v8.7 on Windows 7? Is there a workaround?

 

Many thanks in advance,

 

Arnaud

Labels (1)
0 Kudos
Reply
1 Solution
3,271 Views
kef
Specialist I

I'm not sure if Natep's  solution for CW for S12 V5.0 is applicable for CW for PowerPC:

 https://community.freescale.com/thread/57404

 

But the symptoms were the same - "was interrupted" message. Hope it will work also for CW for PowerPC

 

You need to find working 32bits Win XP machine and install CW there. Then:

 

2) Copy whole CW folder from Win32 machine to Win7 machine (Program Files\CodeWarrior xxxx)

3) Now, this step is the MOST IMPORTANT:

    Look at the file "Mwregsvr.exe" in the c:\Program Files(x86)\Freescale\CodeWarrior for Microcontrollers V6.1\bin and click the right button on this file, then click properties.

    Now, in the compatibility tab,set the compatibility to WindowsXp (sp2) and set the checkbox

    to run in administrator mode.

    Now, click apply button then click OK button.

4) In the same folder, run once the file regservers.bat

    When windows ask for the permisions, just click yes everytime.

 

5)  You may want to create a desktop icon at this point.

 

View solution in original post

0 Kudos
Reply
3 Replies
3,272 Views
kef
Specialist I

I'm not sure if Natep's  solution for CW for S12 V5.0 is applicable for CW for PowerPC:

 https://community.freescale.com/thread/57404

 

But the symptoms were the same - "was interrupted" message. Hope it will work also for CW for PowerPC

 

You need to find working 32bits Win XP machine and install CW there. Then:

 

2) Copy whole CW folder from Win32 machine to Win7 machine (Program Files\CodeWarrior xxxx)

3) Now, this step is the MOST IMPORTANT:

    Look at the file "Mwregsvr.exe" in the c:\Program Files(x86)\Freescale\CodeWarrior for Microcontrollers V6.1\bin and click the right button on this file, then click properties.

    Now, in the compatibility tab,set the compatibility to WindowsXp (sp2) and set the checkbox

    to run in administrator mode.

    Now, click apply button then click OK button.

4) In the same folder, run once the file regservers.bat

    When windows ask for the permisions, just click yes everytime.

 

5)  You may want to create a desktop icon at this point.

 

0 Kudos
Reply
3,271 Views
sbsoccermike
Contributor I

Does anyone know if using SP3 is better or worse than SP2 for this application?

0 Kudos
Reply
3,271 Views
am304
Contributor I

Thanks, that worked a treat!!

 

Arnaud

0 Kudos
Reply