Help with codewarrior 5.1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Help with codewarrior 5.1

1,911 次查看
wzero
Contributor I
Hello, my English is not very good hope that  understand me.
I installed v5.1 codewarrior and spears when the program gives me the following error:

********************************************************************
CodeWarrior encountered an unhandled exception 0x5570d1c9
(the memory at address 0x00000000 could not be read)

Location: MWRADUtils.dll:0x5570d1c9

Crash dump written to c:\Archivos de programa\Freescale\CodeWarrior for HC08
V5.1\bin\IDE.exe.b2015.20071022.162858A.dump

Choose ´abort´ to end the program, 'Retry' to debug, or 'Ignore' to continue (at your own risk)
***************************************************************************************

My PC : S.O windows XP home edition
              250 RAM
              Pentium 4
              HD 100Gigas
my email is dsernesto@yahoo.com
thx.
标签 (1)
0 项奖励
回复
1 回复

618 次查看
CrasyCat
Specialist III
Hello
 
What are you doing when the crash occurs?
Can you provide any reproducible steps...
 
CrasyCat
0 项奖励
回复