Help with codewarrior 5.1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Help with codewarrior 5.1

2,295件の閲覧回数
wzero
Contributor I
Hello, my English is not very good hope that  understand me.
I installed v5.1 codewarrior and spears when the program gives me the following error:

********************************************************************
CodeWarrior encountered an unhandled exception 0x5570d1c9
(the memory at address 0x00000000 could not be read)

Location: MWRADUtils.dll:0x5570d1c9

Crash dump written to c:\Archivos de programa\Freescale\CodeWarrior for HC08
V5.1\bin\IDE.exe.b2015.20071022.162858A.dump

Choose ´abort´ to end the program, 'Retry' to debug, or 'Ignore' to continue (at your own risk)
***************************************************************************************

My PC : S.O windows XP home edition
              250 RAM
              Pentium 4
              HD 100Gigas
my email is [email protected]
thx.
ラベル(1)
0 件の賞賛
返信
1 返信

1,002件の閲覧回数
CrasyCat
Specialist III
Hello
 
What are you doing when the crash occurs?
Can you provide any reproducible steps...
 
CrasyCat
0 件の賞賛
返信