Flash memory with range not definied

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Flash memory with range not definied

2,278 次查看
maurom
Contributor II

Hi,

im ready to Flash my S12 microcontroller through bdm interface and Hiwave.exe. I have saved flash memory in range 0x0e08000 to 0x0e7bfff, but inside it there is some block not defined.

I succeed to save range with (;A) append option in save command, but in the S19 file created there is some hole addresses, same of not defined block.

I need to change some bit in the range0x0e08000 to 0x0e7bfff of saved S19 file and then write changes.

If i try to flash this "holed" S19 file into microcontroller there is possibilitie some go wrong and i loss original memory?

 

Thanks a lot for any replies

Bye

M.

标签 (1)
3 回复数

2,090 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

HI,

What's your chip part number?

you mentioned "I have saved flash memory in range 0x0e08000 to 0x0e7bfff, but inside it there is some block not defined." can you please specify what range of "block" not defined?

Best Regards,

Jennie

2,090 次查看
maurom
Contributor II

Thanks for replie.

Part number is :  MC9S12XE256MAL

In the follow some memory block not defined in range:

0x00E0C00 to 0x00E107F0

0x0E10C00 to 0x0E10FF0

0x0E12000 to 0x0E17FF0

0x0E1C000 to 0x0E207F0

0x0E20C00 to 0x0E20FF0

0x0E22000 to 0x0E27FF0

0x0E2C000 to 0x0E307F0

and more others... if needed i write all memory block range not defined.

Thanks a lot Jennie

0 项奖励
回复

2,090 次查看
maurom
Contributor II

Thanks a lot Jennie, i've posted first of this topic, same question in other section and other people have answered :

https://community.nxp.com/message/839048 

Thanks a lot for your support

Mauro

0 项奖励
回复