MPC83XX : cannot Put the target in DEBUG Mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC83XX : cannot Put the target in DEBUG Mode

2,581件の閲覧回数
parrepati
Contributor I

Hi every one,

I am working with MPC8378 Borad and im using CODEWARRIOR V8.8. when i tried to connect i m getting error msg like

CCSprotocolpulgin : Failed to reset the Target

MPC83XX : cannot Put the target in DEBUG Mode

can you help me in this issue

thanks in advance.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,968件の閲覧回数
J2MEJediMaster
Specialist I

What MPC board are you using, and does it show up in the CodeWarrior wizard when you create a CodeWarrior project?

 

Have you installed all service packs?

 

---Tom

0 件の賞賛
返信

1,968件の閲覧回数
Freshman
Contributor III

I have the same problem ,Tom ,  can you  help me?

I use the MPC8313ERDB ,  and I have setted it and installed all service packs ! 

What's wrong ?

thank you in advance

--Kevin

0 件の賞賛
返信

1,968件の閲覧回数
李鹏斌
Contributor II

Did you solve the problem?

0 件の賞賛
返信