Extended ASCII characters

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Extended ASCII characters

ソリューションへジャンプ
5,184件の閲覧回数
FredF
Contributor III

I am using CW8.2.2 with IDE 5.6.1, and I need to use 8-bit ASCII characters beyond 0x7F.  However, there are inconsistencies between the way the IDE and the compiler represent the characters.  For example, if a capital C with cedilla 'Ç' is entered in the IDE using the traditional value 0x80, it is displayed properly.  When this character is compiled as part of a string, it is given the value 0xC7, which is a valid value using a newer extended ASCII table, but not the same as 0x80.  Is there a way to get the IDE and compiler to use the same extended ASCII table?

 

Thanks,

 

Fred

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,935件の閲覧回数
FredF
Contributor III

Thanks for the response, but I was able to resolve the issue.  In Windows with a full keyboard, holding the ALT key and entering 1-2-8 (0x80) on the keypad will produce Ç using the 8859 character set.  Holding the ALT key and entering 0-1-9-9 will produce Ç using the 8859-1 character set.  The compiler uses the 8859-1 character set, so creating strings with the 0-x-x-x codes produce the correct hex values when compiled.  However, the CW IDE does not recognize all the extended ASCII characters when they are entered, so an alternate editor may be required.  Once they are entered in the file, the IDE displays them correctly, and they are compiled correctly. 

 

Thanks,

 

Fred

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,935件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi,

 

There are 2 norms for extended ASCII table:

  - ISO-8859

  - ISO-8859-1 for Latin Europe.

 

We need more details when you said:

For example, if a capital C with cedilla 'Ç' is entered in the IDE using the traditional value 0x80, it is displayed properly.

How do you entered it in the IDE ?

 

What is the Windows OS used ?

Is it the US version ?

 

Do you have an example reproducing the behavior ?

 

Regards

Pascal

0 件の賞賛
返信
2,936件の閲覧回数
FredF
Contributor III

Thanks for the response, but I was able to resolve the issue.  In Windows with a full keyboard, holding the ALT key and entering 1-2-8 (0x80) on the keypad will produce Ç using the 8859 character set.  Holding the ALT key and entering 0-1-9-9 will produce Ç using the 8859-1 character set.  The compiler uses the 8859-1 character set, so creating strings with the 0-x-x-x codes produce the correct hex values when compiled.  However, the CW IDE does not recognize all the extended ASCII characters when they are entered, so an alternate editor may be required.  Once they are entered in the file, the IDE displays them correctly, and they are compiled correctly. 

 

Thanks,

 

Fred

0 件の賞賛
返信