Debugging for CodeWarrior 9 on Leopard

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debugging for CodeWarrior 9 on Leopard

2,632件の閲覧回数
Rafish
Contributor I
Hello all,

I've been using CW9 on a MOtorolla based mac running OSX 10.4.10. When I switched to a new iMac (2.0 GHz core 2 duo) running Leopard (10.5.2) the debugger of CW9 didn't work. I know it needs XCode to run it, and I have installed Xcode 3 for it but it doesn't work. Unfortunately I can't use the same old software (older OS, Xcode 2) because it can't be installed on the new mac. What can I do ?

Rafi.
ラベル(1)
0 件の賞賛
返信
1 返信

1,094件の閲覧回数
J2MEJediMaster
Specialist I
CodeWarrior for Mac OS is no longer supported, and hasn't been for some time. You're going to have to start migrating your code to XCode.

---Tom

0 件の賞賛
返信