prescale timer -ADC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

prescale timer -ADC

2,978 Views
Halom
Contributor I
Hi ,
I would like to know how should I prescale the AD converter if the timer has been prescale at 4 Mhz instead to 8 Mhz. 
I am using the MC9S12C32 in a program involving timer interrupt.
 I have some problem to understand it because the ADC has a max clock of 2 Mhz.
 
Thank you
 
Labels (1)
0 Kudos
Reply
1 Reply

1,155 Views
kef
Specialist I
You should select ATD prescaler so that busclock divided by prescaler is not higher than 2MHz (see ATD specs) and not less than 0.5MHz (again see ATD specs).
Suppose you use 8MHz crystal and no PLL. Then busclock is 4MHz. You can divide this at least by 2 and 2MHz. At the other hand you can divide 4MHz bus clock not more than 8 times, 4MHz /8=0.5MHz.
In datasheet table 8-8 you may see that Prescale Value bits are from binary 00000 to 00011.
0 Kudos
Reply