Debugging for CodeWarrior 9 on Leopard

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Debugging for CodeWarrior 9 on Leopard

2,609 次查看
Rafish
Contributor I
Hello all,

I've been using CW9 on a MOtorolla based mac running OSX 10.4.10. When I switched to a new iMac (2.0 GHz core 2 duo) running Leopard (10.5.2) the debugger of CW9 didn't work. I know it needs XCode to run it, and I have installed Xcode 3 for it but it doesn't work. Unfortunately I can't use the same old software (older OS, Xcode 2) because it can't be installed on the new mac. What can I do ?

Rafi.
标签 (1)
0 项奖励
回复
1 回复

1,071 次查看
J2MEJediMaster
Specialist I
CodeWarrior for Mac OS is no longer supported, and hasn't been for some time. You're going to have to start migrating your code to XCode.

---Tom

0 项奖励
回复