Cyclone Universal programing CW6.3 s-record file issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cyclone Universal programing CW6.3 s-record file issue

1,451 Views
dannydeng
Contributor III

Dears,

  I found the issue when I use Cyclone Universal programing CW6.3 s-record file of S9S08DZ60F2MLH, it appeared some mistake 0x00003003 at the Flash address 0x0000F400. While programing CW10.x s-record file, it is well.

   Can anybody give any advice?

  Thanks and best regards,

Ray Deng,

0 Kudos
Reply
3 Replies

1,171 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Ray,

If your srecord file is generated by CW, please verify the file with CW debugger if its function is correct.

If yes, srecord file is fine. I suggest you contact Cyclone Universal producer P&E.

PEmicro - P&E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Develop... 


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,171 Views
dannydeng
Contributor III

Hi Jennie,

    Thanks for your kinldy suggestion.

   I will check it.

Thanks and best regards,

Ray Deng

0 Kudos
Reply

1,171 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

You are welcome!

Have a great day,
Jennie Zhang

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply