Cyclone Universal programing CW6.3 s-record file issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cyclone Universal programing CW6.3 s-record file issue

2,035件の閲覧回数
dannydeng
Contributor III

Dears,

  I found the issue when I use Cyclone Universal programing CW6.3 s-record file of S9S08DZ60F2MLH, it appeared some mistake 0x00003003 at the Flash address 0x0000F400. While programing CW10.x s-record file, it is well.

   Can anybody give any advice?

  Thanks and best regards,

Ray Deng,

0 件の賞賛
返信
3 返答(返信)

1,755件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Ray,

If your srecord file is generated by CW, please verify the file with CW debugger if its function is correct.

If yes, srecord file is fine. I suggest you contact Cyclone Universal producer P&E.

PEmicro - P&E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Develop... 


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,755件の閲覧回数
dannydeng
Contributor III

Hi Jennie,

    Thanks for your kinldy suggestion.

   I will check it.

Thanks and best regards,

Ray Deng

0 件の賞賛
返信

1,755件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

You are welcome!

Have a great day,
Jennie Zhang

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信