Codewarrior sofware information?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrior sofware information?

4,943件の閲覧回数
javi
Contributor I
Dear All,
 
I am new to codewarrior software package. I would like to learn it using the HCS8, the DSP56XXX and Coldfires from freescale. But, here come my question: Do I need to install three different codewarrior softwares?. I mean, one for the HCS8, other for Coldfire and another for the DSP56XXX?. Or I just need to install One codewarrior software because it includes all these other options?.
 
Thanks a lot and best regards,
 
Javi
ラベル(1)
0 件の賞賛
返信
1 返信

2,194件の閲覧回数
BlackNight
NXP Employee
NXP Employee
Hello,
no, you will need to install CodeWarrior for each respective portfolio (DSP, Coldfire or HC08). They share the same IDE/UI. Technically you could install them all into one installation on your machine, but this is not recommended for non-expert users.

While it would be possible to have one installation providing support for DSP + Coldfire + HC08, this has not turned out beeing much practical as the silicon roadmaps are different, and it would increase the installation image size for download. But I'm sure Freescale is thinking about ways to get around this too for the future.

Thanks,
Erich
0 件の賞賛
返信