Codewarrior does not like teamcity

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrior does not like teamcity

1,218件の閲覧回数
SamK
Contributor I

Hello

 

   I have been running builds from teamcity using Ant/build.xml that launch codewarrior and do a build.  Most of the times (9 out of 10), codewarrior will crash with a exception message.  The build running on teamcity hangs indefinitely until I log into the windows xp virtual machine and click on 'ok'.  

 

  however, without making any changes to anything, if I kick off the build again, it passes just fine.  I have tried rebooting the machine before doing the build as well but its to no use.  Any idea what could be causing it to crash?  

 

  the teamcity build log has no useful information:

for.family.build:

[echo] Trying to compile EPG lib target = epg_lib 

and then it hangs.


This is the log file on windows:
[echo] Trying to compile EPG lib target = epg_lib
     [exec] Current OS is Windows XP
     [exec] Executing 'c:\Program Files\Metrowerks\CodeWarrior\Bin\IDE.exe' with arguments:
'/t'
'epg_lib'
'/b'
'/c'
'Build.mcp'
 
ラベル(1)
0 件の賞賛
返信
1 返信

1,068件の閲覧回数
SamK
Contributor I

My version of codewarrior is 4.2.6.862

 

I am running it on Windoze XP SP3 AMD Opteron Processor 6174 

 

thanks

0 件の賞賛
返信