CodeWarrior2.7 + Lauterbach USB-JTAG on MPC5604B

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior2.7 + Lauterbach USB-JTAG on MPC5604B

2,936件の閲覧回数
SylvainBortelle
Contributor I

Hello,

 

I just created an executable (.elf) with CodeWarrior 2.7, and I would like to know if it works.

 

I try to use Lauterbach for connected Computer-Eval Board. The name of this is : "Debuger USB2 Power debug interface". I have installed it, but CodeWarrior dont detect him.

 

Can you help me for found out if i forgot someting.

 

Thank you.

 

Best regard.

ラベル(1)
0 件の賞賛
返信
6 返答(返信)

2,453件の閲覧回数
J2MEJediMaster
Specialist I

What version of Windows are you running?

Did you install the drivers for the Lauterbach run control device?

 

---Tom

0 件の賞賛
返信

2,453件の閲覧回数
SylvainBortelle
Contributor I

Thank you for your help.

 

I use Windows XP (SP3).

 

I installed the driver for Launterbach run control device. He works well with Trace32.

0 件の賞賛
返信

2,453件の閲覧回数
J2MEJediMaster
Specialist I

In CodeWarrior, have you checked all of the debugger settings panels? Specifically,  there should be some remote debug settings or connection settings where you choose the run-control device/interface. Is the Lauterbach visible there?

 

Sorry I can't be more specific because I don't have that version of CodeWarrior.

 

---Tom

0 件の賞賛
返信

2,453件の閲覧回数
SylvainBortelle
Contributor I

Sorry but i don't undersand what is for you: "the debugger settings panels" ?

 

In "Edit/Preference...", I don't find any information about a debugger settings panels.

 

After a successful compilation, a pop-up opens. In this pop-up there is a combo box with 5 choose:

  • CABPPCNEXUS, Connected via Parallel Port or BDM Lightning
  • USB Multilink, Embedded Multilink, or Embedded OSJTag
  • Cyclone MAX - Serial Port
  • Cyclone MAX - Ethernel Port
  • Cyclone MAX - USB Port

I can't find Lauterbach.

 

Thank you for your help and good week.

0 件の賞賛
返信

2,453件の閲覧回数
J2MEJediMaster
Specialist I

You probably don't see any debugger settings panels because CodewWarrior hasn't found a debug probe yet. According to this Freescale page, Lauterbach probes are supported. The only choice that makes sense is the PPCNEXUS one. This same page also advises when using a Lauterbach: "Please read TargetingMPC55xx.pdf located in the Help\pdf folder of your CodeWarrior installation."

 

---Tom

0 件の賞賛
返信

2,453件の閲覧回数
SylvainBortelle
Contributor I

Indeed, a solution is described here: TargetingMPC55xx.pdf, page 79. We must create a .cmm file to use CodeWarrior and Lauterbach together. Unfortunately I can't integrate with an existing project...

 

Again thank you for your help. Good day.

0 件の賞賛
返信