Codewarrior does not like teamcity

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior does not like teamcity

1,229 Views
SamK
Contributor I

Hello

 

   I have been running builds from teamcity using Ant/build.xml that launch codewarrior and do a build.  Most of the times (9 out of 10), codewarrior will crash with a exception message.  The build running on teamcity hangs indefinitely until I log into the windows xp virtual machine and click on 'ok'.  

 

  however, without making any changes to anything, if I kick off the build again, it passes just fine.  I have tried rebooting the machine before doing the build as well but its to no use.  Any idea what could be causing it to crash?  

 

  the teamcity build log has no useful information:

for.family.build:

[echo] Trying to compile EPG lib target = epg_lib 

and then it hangs.


This is the log file on windows:
[echo] Trying to compile EPG lib target = epg_lib
     [exec] Current OS is Windows XP
     [exec] Executing 'c:\Program Files\Metrowerks\CodeWarrior\Bin\IDE.exe' with arguments:
'/t'
'epg_lib'
'/b'
'/c'
'Build.mcp'
 
Labels (1)
0 Kudos
Reply
1 Reply

1,079 Views
SamK
Contributor I

My version of codewarrior is 4.2.6.862

 

I am running it on Windoze XP SP3 AMD Opteron Processor 6174 

 

thanks

0 Kudos
Reply