Codewarrior Error : encountered an unhandled exception 0xc0000005 => HELP please

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior Error : encountered an unhandled exception 0xc0000005 => HELP please

4,210 Views
hasaur
Contributor II

Hello,

I was using Codewarrior for 8bits and 16bits MCU and I never had problem. I was using it yesterday without any problem.

But this morning, when I started both Codewarrior for 8 and 16 bits I had an error and that is the case each time I start it. I have tried to delete it and install it but it is the same thing.

 

Please help me I don't know what it can be, I didn't do something new.

 

Thank you

Labels (1)
0 Kudos
Reply
3 Replies

2,150 Views
J2MEJediMaster
Specialist I

Are you using the CodeWarrior for MCUs 10 beta?

 

---Tom

0 Kudos
Reply

2,150 Views
hasaur
Contributor II

Hello,

I have installed this version : http://cache.freescale.com/lgfiles/devsuites/HC08/CW_MCU_V6_3_SE.exe?WT_TYPE=IDE%20-%20Debug,%20Comp...

 

now, after deleting and reinstalling the software 2 times, codewarrior works (but I don't know why it did this error, I didn't do something anormal), but now, it's the OSBDM that doesn't want to work. I have deleted the driver but I can't find it. The problem is that I can't remind how I did it the first time to make it work and I don't know what is the model. I think it is JM60.

Is there driver for this device ?

 

Thank you.

0 Kudos
Reply

2,150 Views
hasaur
Contributor II

I have founded the driver and now all works fine.

But I don't know if I will had this codewarrior problem another time...

0 Kudos
Reply