Codewarrior 6.2.2 patch file

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Codewarrior 6.2.2 patch file

跳至解决方案
2,709 次查看
nbgatgi
Contributor IV

The link provided by NXP for legacy download support doesn't work.  Does anyone have the 6.2.2 compiler patch file?

For reference, here is the link for the download that is failing.  I need the top and 3rd from top items.

Updates for CodeWarrior for Microcontrollers v6.2|NXP 

Thanks!

0 项奖励
回复
1 解答
2,369 次查看
nbgatgi
Contributor IV

After speaking with a former NXP FAE, I was directed to the download link for 6.2 SE.  This has allowed me to install the patch provided by Alice_Yang earlier in the thread.  Here is the link for the 6.2 SE download ... You need to select "More" in order to find the correct download link at the bottom of the list.

CodeWarrior® Development Tools Suite - Special|NXP 

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,369 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Nick,

 

There is some problem on the link, I reported it to related team, they are still working on it.

While My colleague Jennie Zhang shared the path for you , it is too large to can't attach it

in this community, so please download it from the google drive:

https://drive.google.com/file/d/11eBKdUY1DnepoVNPmNp_zgWY68DCnXFT/view  

 


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,368 次查看
nbgatgi
Contributor IV

Alice,

Thank you for posting the patch file.  I was able to download and run it which led me to a new problem.  I believe what I am calling version 6.2 is not the same as the 6.2 the patch is associated with.  When I attempted to install the patch, I received an error:

CW 6_2_2 patch fail.png

Note the path of the Code Warrior install that I pointed to.  I assume that the indication of it being "... for  ColdFire ... " might be the issue.

To get at what I REALLY need, I have attached the version details from the system our code was developed on.  You might be wondering, why I don't just use that system.  The problem is that the system is at our division in France and we are in Wisconsin, USA.  Apparently, sending that system is not an option for various reasons.

Hoping you can help soon!

0 项奖励
回复
2,370 次查看
nbgatgi
Contributor IV

After speaking with a former NXP FAE, I was directed to the download link for 6.2 SE.  This has allowed me to install the patch provided by Alice_Yang earlier in the thread.  Here is the link for the 6.2 SE download ... You need to select "More" in order to find the correct download link at the bottom of the list.

CodeWarrior® Development Tools Suite - Special|NXP 

0 项奖励
回复
2,368 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Nick,

Thanks for your sharing.

Have a nice day,

Alice

0 项奖励
回复