Codewarrior 10.2 questions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrior 10.2 questions

1,822件の閲覧回数
Teckna
Contributor V

Hi everyone,

 

I downloaded and installed CW 10.2. Now I have two question:

 

  1. I have a CW 10.1 license working on my PC: if I run CW 10.1 it works fine, if I run CW 10.2 it works ok, but it shows that I'm working with an evaluation license that will expire in 30 days. Have I to get a purchase a new license to make the CW 10.2 work with no limitation at the end of the evaluation period? If no, which are the steps to do to upgrade the license to CW 10.2?
  2. In CW 10.2 I cannot create a new MQX (3.8) project, there is no item in the list of the new project wizard that enables me to create a new MQX 3.8 project. I tried to uninstall and reinstall MQX 3.8, thinking it would install the MQX extension to CW 10.2, but with no success. Is there some manual step to do to make it work?

Many thanks

Teckna

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,154件の閲覧回数
Teckna
Contributor V

I found the solution for the question 2 in this post (it's relative to CW 10.1).

 

https://community.freescale.com/message/101996#101996

 

Teckna

0 件の賞賛
返信

1,154件の閲覧回数
CrasyCat
Specialist III

Hello

 

On question 1:

Check following bog post "http://mcuoneclipse.wordpress.com/2012/02/06/mcu10-2-is-here-or-4-t-shirts-in-13-weeks/"

 

It looks like 10.2 uses an updated license key. As a registered owner with current support you should be able to get this at no additional costs. If the free special edition is good enough, then things are even easier as it comes with a special edition license for free.

 

CrasyCat

0 件の賞賛
返信