Codewarrior 10.2 questions

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior 10.2 questions

1,824 Views
Teckna
Contributor V

Hi everyone,

 

I downloaded and installed CW 10.2. Now I have two question:

 

  1. I have a CW 10.1 license working on my PC: if I run CW 10.1 it works fine, if I run CW 10.2 it works ok, but it shows that I'm working with an evaluation license that will expire in 30 days. Have I to get a purchase a new license to make the CW 10.2 work with no limitation at the end of the evaluation period? If no, which are the steps to do to upgrade the license to CW 10.2?
  2. In CW 10.2 I cannot create a new MQX (3.8) project, there is no item in the list of the new project wizard that enables me to create a new MQX 3.8 project. I tried to uninstall and reinstall MQX 3.8, thinking it would install the MQX extension to CW 10.2, but with no success. Is there some manual step to do to make it work?

Many thanks

Teckna

Labels (1)
0 Kudos
Reply
2 Replies

1,156 Views
Teckna
Contributor V

I found the solution for the question 2 in this post (it's relative to CW 10.1).

 

https://community.freescale.com/message/101996#101996

 

Teckna

0 Kudos
Reply

1,156 Views
CrasyCat
Specialist III

Hello

 

On question 1:

Check following bog post "http://mcuoneclipse.wordpress.com/2012/02/06/mcu10-2-is-here-or-4-t-shirts-in-13-weeks/"

 

It looks like 10.2 uses an updated license key. As a registered owner with current support you should be able to get this at no additional costs. If the free special edition is good enough, then things are even easier as it comes with a special edition license for free.

 

CrasyCat

0 Kudos
Reply