CodeWarrior for QorIQ Qonverge Platform

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior for QorIQ Qonverge Platform

1,746件の閲覧回数
NeenaB
Contributor I

Hi..

 

Which version of CodeWarrior supports QorIQ Qonverge Platform - PSC9131?.. Can i use CodeWarrior for Power Architecture for this as it supports only e500 core and PSC9131 contains both e500 and sc3850 cores?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,481件の閲覧回数
J2MEJediMaster
Specialist I

You would use CodeWarrior for Power Architecture to debug the e500 core and CodeWarrior for StarCore in tandem to debug the SC3850 core. For further information, please check with your Freescale representative.

 

---Tom

0 件の賞賛
返信

1,481件の閲覧回数
NeenaB
Contributor I

I have connected PSC9131RDB. Actually in CodeWarrior Power Architecture 10.1.1, PSC9131 is not mentioned in the list of supported devices. So i selected P1010 as it contains single e500 core. With that configuration, i am able to bulid successfully. Bt when i tried 2 debug, at the end of debug session following error is gettin displayed :

 

Failed to resume target process., CCSProtocolPlugin :  [CCS last error: USB open failure ]

 

How can i rectify this so that i can run my code in e500 core with PSC9131RDB using the IDE CodeWarrior Power Architecture 10.1.1?..

0 件の賞賛
返信

1,481件の閲覧回数
J2MEJediMaster
Specialist I

You need to install the Service Pack for PSC9131 into your copy of CodeWarrior for Power Architecture. This is not a public download; see your Freescale representative for how to obtain this service pack.

 

---Tom

 

0 件の賞賛
返信