MC56F8037 in-circuit debug interfaces problems

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC56F8037 in-circuit debug interfaces problems

1,615件の閲覧回数
AlanPas
Contributor I

Hi all,

 

I'm starting developing fw for MC56F8037 DSC, I downloaded CW 8.3SE and as a programming/debugging interface I can choose from Codewarrior USB TAP and PEmicro USB Universal Multilink, but none of them works.

 

When I try to enter debug mode with USB TAP (that seems to be correctly configured in Debugger Settings panel), I've got error message : "CCS: Library not found".

 

With the Universal Multilink, I can't select it from CW 8.3 available interfaces.

 

What should I do?

What Development tool and what interface do you suggest me to use?

 

Thank you

Alan

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,251件の閲覧回数
Law
Contributor I

Hiya,

 

I have been developing on the MC56F8037 EVM using the USB TAP successfully. On Windows XP, mind you.

 

One thing I have found is when I create a new project, there is a button next to the build selector (right name??) i.e. where I can select SDM_pFlash / SDM_Simulator / Build all. When I mouse over it, it appears as "SDM_pFlash Settings".

 

Anyway, If I click that, in the Debugger\Remote Debugging selection, I have to select 56800E Local USBTAP Connection before I have any luck. If you select that, and click Edit Connection, just make sure the Connection Type is set to "USB TAP Connection." I didnt have to change any settings.

 

Failing that, check under edit\ Preferences - Debugger\Remote Connections that the USB TAP appears in there.

 

Good Luck!

 

Laurence

0 件の賞賛
返信