CodeWarrior for QorIQ Qonverge Platform

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior for QorIQ Qonverge Platform

1,732 Views
NeenaB
Contributor I

Hi..

 

Which version of CodeWarrior supports QorIQ Qonverge Platform - PSC9131?.. Can i use CodeWarrior for Power Architecture for this as it supports only e500 core and PSC9131 contains both e500 and sc3850 cores?

Labels (1)
0 Kudos
Reply
3 Replies

1,467 Views
J2MEJediMaster
Specialist I

You would use CodeWarrior for Power Architecture to debug the e500 core and CodeWarrior for StarCore in tandem to debug the SC3850 core. For further information, please check with your Freescale representative.

 

---Tom

0 Kudos
Reply

1,467 Views
NeenaB
Contributor I

I have connected PSC9131RDB. Actually in CodeWarrior Power Architecture 10.1.1, PSC9131 is not mentioned in the list of supported devices. So i selected P1010 as it contains single e500 core. With that configuration, i am able to bulid successfully. Bt when i tried 2 debug, at the end of debug session following error is gettin displayed :

 

Failed to resume target process., CCSProtocolPlugin :  [CCS last error: USB open failure ]

 

How can i rectify this so that i can run my code in e500 core with PSC9131RDB using the IDE CodeWarrior Power Architecture 10.1.1?..

0 Kudos
Reply

1,467 Views
J2MEJediMaster
Specialist I

You need to install the Service Pack for PSC9131 into your copy of CodeWarrior for Power Architecture. This is not a public download; see your Freescale representative for how to obtain this service pack.

 

---Tom

 

0 Kudos
Reply