CodeWarrior Running on a Mac

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior Running on a Mac

2,699 Views
Wings
Contributor I
If anyone is interested or curious, CW 5.1 and P&E (Hiwave?) debugger seem to run just fine using a MacBook (C2D) running Parallels with Windows XP Pro. My connection to the target system is USB2 to a Cyclone Pro.

In addition, all CW files are on a networked drive located on my desktop Mac and that works without a hitch.

I used to run CW on the MacBook by booting directly into XP via Bootcamp, but I just got Parallels and everything seems to run just fine with that. Much better solution than having to reboot to run CW. Plus, Windows is pretty much in a sandbox on the Macbook.

(To edit, I use my favorite editor, SubEthaEdit (what a name), on the desktop Mac and the edits are picked up just fine in CW.)

I'm almost a happy camper now.
Labels (1)
0 Kudos
Reply
1 Reply

1,248 Views
FastEddie
Contributor I
I just dowloaded the trial version of Code Warrior for my M52233DEMO board. I keep getting the error message PEMicroProtocaolPlugin: No USB Connection found. I have gone into parallels to enable the USB port and to use AutoConnect. I have waited to plug in the eval board until parallels is up and Windows is booted. Any suggestions would be helpful.






Wings wrote:
If anyone is interested or curious, CW 5.1 and P&E (Hiwave?) debugger seem to run just fine using a MacBook (C2D) running Parallels with Windows XP Pro. My connection to the target system is USB2 to a Cyclone Pro.

In addition, all CW files are on a networked drive located on my desktop Mac and that works without a hitch.

I used to run CW on the MacBook by booting directly into XP via Bootcamp, but I just got Parallels and everything seems to run just fine with that. Much better solution than having to reboot to run CW. Plus, Windows is pretty much in a sandbox on the Macbook.

(To edit, I use my favorite editor, SubEthaEdit (what a name), on the desktop Mac and the edits are picked up just fine in CW.)

I'm almost a happy camper now.


0 Kudos
Reply