CodeWarrior Hardware Breakpoints

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior Hardware Breakpoints

2,770件の閲覧回数
davidcav
Contributor II
I am using CodeWarrior to debug a MC68332 CPU board.  My code is running in Flash ROM.  The datasheet for the MC68332 indicates that I should be able to set up to 4 hardware breakpoints, however, when I try to set one, I always get the following message from CodeWarrior:
 
"Maximum number of hardware breakpoints (1) has been reached"
 
I do not see any  breakpoints set when I "View -> Breakpoints"  from the codeWarrior.  I am using the P&E Micro BDM debugger to connect to my board.  
 
Is there a certain configuration, or register setting that is unenabling hardware breakpoints??
ラベル(1)
0 件の賞賛
返信
1 返信

1,332件の閲覧回数
Nouchi
Senior Contributor II
Hello,

As far as remember, there's no hardware breakpoint support (except BKPT pin) on MC68332.
IMHO, the best thing to do, is to move your code to ram and use software breakpoints.
But I could be wrong, because I never used CW with 68332, I used an old Hiware compiler with the older BMdebug debugger.


Emmanuel,
0 件の賞賛
返信