CodeWarrior Hardware Breakpoints

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CodeWarrior Hardware Breakpoints

2,275 次查看
davidcav
Contributor II
I am using CodeWarrior to debug a MC68332 CPU board.  My code is running in Flash ROM.  The datasheet for the MC68332 indicates that I should be able to set up to 4 hardware breakpoints, however, when I try to set one, I always get the following message from CodeWarrior:
 
"Maximum number of hardware breakpoints (1) has been reached"
 
I do not see any  breakpoints set when I "View -> Breakpoints"  from the codeWarrior.  I am using the P&E Micro BDM debugger to connect to my board.  
 
Is there a certain configuration, or register setting that is unenabling hardware breakpoints??
标签 (1)
0 项奖励
回复
1 回复

837 次查看
Nouchi
Senior Contributor II
Hello,

As far as remember, there's no hardware breakpoint support (except BKPT pin) on MC68332.
IMHO, the best thing to do, is to move your code to ram and use software breakpoints.
But I could be wrong, because I never used CW with 68332, I used an old Hiware compiler with the older BMdebug debugger.


Emmanuel,
0 项奖励
回复