CodeWarrior Dev Studio for ColdFire  v5.1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior Dev Studio for ColdFire  v5.1

ソリューションへジャンプ
2,575件の閲覧回数
ryanfauth
Contributor I

I need to use CodeWarrior Dev Studio for ColdFire  v5.1 for a legacy project.  Where can I find this?

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 解決策
2,273件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello Ryan.

all Freescale available CodeWarrior Legacy Downloads are listed here:

CodeWarrior Legacy Downloads|Freescale

However CodeWarrior Dev Studio for ColdFire  v5.1 is a very old version ( released before 2005) and it is no longer available on Freescale web site. I don;t know why you want to use that old CW? what chip do you work with? if you use Coldfire V2-V4 derivatives, please use CW v7.2 or CWv10.6 instead:

http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_SPECIALEDITIONS

thus if you have any CW related question with CW v7.2 or CWv10.6, Freescale is still easy to provide support.

can this help?


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,274件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello Ryan.

all Freescale available CodeWarrior Legacy Downloads are listed here:

CodeWarrior Legacy Downloads|Freescale

However CodeWarrior Dev Studio for ColdFire  v5.1 is a very old version ( released before 2005) and it is no longer available on Freescale web site. I don;t know why you want to use that old CW? what chip do you work with? if you use Coldfire V2-V4 derivatives, please use CW v7.2 or CWv10.6 instead:

http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_SPECIALEDITIONS

thus if you have any CW related question with CW v7.2 or CWv10.6, Freescale is still easy to provide support.

can this help?


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,273件の閲覧回数
ryanfauth
Contributor I

Thanks for your reply,

My goal is to use a newer version of the IDE.  The firmware I am working with was originally built with ver5.1 and I would like to confirm that my build environment is correct by first building the project using the original IDE.

I am using CW ver7.2 now.   Is it possible you could send me a copy of ver5.1 that I could run my  preliminary test with?  ( I understand there is no support for this product)

0 件の賞賛
返信
2,273件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Ryan,

The older versions are not available on Web site.

I need to upload the version on pour transweb system.

For tracking ... I will create a SR for this question.


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信