CodeWarrior Debugger Callstack

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior Debugger Callstack

3,837 Views
ignisuti
Contributor IV

I'm using CW10.2 on a Windows 7 64-bit machine


At some point, I had a View in my Debugger that showed me a Callstack. It was called something else and I can't seem to remember what it was called.

 

Does anyone know. I really miss it...

Labels (1)
0 Kudos
Reply
7 Replies

3,463 Views
CrasyCat
Specialist III

Hello

 

    Inside of Eclipse you usually see the call stack in the Debug View

 

CrasyCat

0 Kudos
Reply

3,463 Views
ignisuti
Contributor IV

Yes, that's correct, but I closed that window at some point and can't remember what it was called.

0 Kudos
Reply

3,463 Views
CrasyCat
Specialist III

Hello

 

In order to re-open it:

    - Select Window > Show View > Other.

    - Expand the Debug tree

    - Click on Debug.

 

CrasyCat

0 Kudos
Reply

3,463 Views
ignisuti
Contributor IV

Yes, that didn't do it. The Debug Perspective USED to have the Callstack VIEW. Only it wasn't called Callstack, it was called something else that I can't remember. 

 

Resetting my Debug Perspective doesn't help because I've saved the Debug perspective after I closed the Callstack view. Hindsight makes me really wish I hadn't done that, but it should be easy to get the Callstack back if I only knew what it was called.

0 Kudos
Reply

3,463 Views
CrasyCat
Specialist III

Hello

 

    I have no clue which view you are talking about here.

   I am always getting the Call stack inside the Debug View.

 

    Did you consider creating a new Workspace and importing your project there?

    This should allow you to return back to the default layout for the debug perspective.

 

    To create a new workspace, select File > Switch Workspace > Other and browse for a new workspace location.

    This way you should be able at least to retrieve the name of the view you are looking for.

 

CrasyCat

0 Kudos
Reply

3,463 Views
ignisuti
Contributor IV

CrasyCat, you were right all along. I was getting something confused. 

 

Please accept my sincere apologies.

0 Kudos
Reply

3,463 Views
CrasyCat
Specialist III

Hello

 

No problem. I am glad you get up and running again.

 

CrasyCat

0 Kudos
Reply