CodeWarrior 10 linker call problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior 10 linker call problem

1,858 Views
aersek
Contributor I

I have found problem with linker invication in CW 10 for windows. This is problem logg:

 

'Invoking: ColdFire Linker'
"C:\Program Files\Freescale\CW MCU v10.0\eclipse\../MCU_10.0/ColdFire_Tools/Command_Line_Tools/mwldmcf" -sym full -msgstyle gcc -proc 5282 -nostdlib "D:/CFdemo/utasker_sisco/Applications/uTaskerV1.4/CodeWarrior_M5223X/uTaskerV1.4_CW7/..\cfg\dmk105.lcf" -m start -L"D:/CFdemo/utasker_sisco/Applications/uTaskerV1.4/CodeWarrior_M5223X/uTaskerV1.4_CW7/..\bin\" -application -map -srec -sreclength 32 -sreceol dos -list -w on -o "..\..\bin\uTasker_full.elf"  "./uTasker/Driver.obj" "./uTasker/GlobalTimer.obj" "./uTasker/Tty_drv.obj" "./uTasker/USB_drv.obj" "./uTasker/Watchdog.obj" "./uTasker/can_drv.obj" "./uTasker/eth_drv.obj" "./uTasker/iic_drv.obj" "./uTasker/low_power.obj" "./uTasker/uFile.obj" "./uTasker/uMalloc.obj" "./uTasker/uNetwork.obj" "./uTasker/uTasker.obj"  "./uTasker/uGLCDLIB/GLCD.obj"  "./uTasker/MODBUS/MODBUS.obj"  "./TCP_IP/Ethernet.obj" "./TCP_IP/NetBIOS.obj" "./TCP_IP/arp.obj" "./TCP_IP/dhcp.obj" "./TCP_IP/dns.obj" "./TCP_IP/ftp.obj" "./TCP_IP/http.obj" "./TCP_IP/icmp.obj" "./TCP_IP/ip.obj" "./TCP_IP/ip_utils.obj" "./TCP_IP/pop3.obj" "./TCP_IP/ppp.obj" "./TCP_IP/smtp.obj" "./TCP_IP/snmp.obj" "./TCP_IP/tcp.obj" "./TCP_IP/telnet.obj" "./TCP_IP/tftp.obj" "./TCP_IP/udp.obj" "./TCP_IP/webutils.obj"  "./Source/KeyScan.obj" "./Source/LCD.obj" "./Source/NetworkIndicator.obj" "./Source/application.obj" "./Source/debug.obj" "./Source/modbus_app.obj" "./Source/usb_application.obj" "./Source/webInterface.obj"  "./Hardware/M5223X.obj" "./Hardware/Startup.obj"  "./DIRTOS/D105OSB5.obj" "./DIRTOS/OS_AP_CF.obj" "./DIRTOS/SYS_CNST.obj"  "./BSD/BSD.obj" "./BSD/assert.obj" "./BSD/function.obj" "./BSD/malloc.obj" "./BSD/printf.obj" "./BSD/qsort.obj"   
### ../MCU_10.0/ColdFire_Tools/Command_Line_Tools/mwldmcf Usage Error:

#   Filename or directory '...SD/printf.obj ./BSD/qsort.obj   ' is too long,

#   expected maximum 260 characters
C:\Program Files\Freescale\CW MCU v10.0\gnu\bin\make: *** [../../bin/uTasker_full.elf] Error 1

 

Is there any solution for this problem? I tried to make paths shorter but problem persist.

 

Regards

 

Andrija Ersek

Labels (1)
0 Kudos
Reply
1 Reply

1,025 Views
CrasyCat
Specialist III

Hello

 

In order to report a problem in CodeWarrior V10 for MCU I would recommend you to follow the official path.

 

Instructions on how to report a problem in MCU10 are documented at

  http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MCU10&tid=CWHms

Just click on the link "Instructions for entering a Service Request" there.

 

 

CrasyCat

0 Kudos
Reply