Code Warrior 10 - failed connection to P&E USB Multilink Interface rev C

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code Warrior 10 - failed connection to P&E USB Multilink Interface rev C

2,389 Views
jorgen
Contributor I

I have installed the Code Warrior 10 on Windows 7 (32 bit). I have attached the P&E USB Multilink Interface Rev C to my PC and to the taget (an MC9S08SV16).

 

I have a program in C that compiles and builds without errors.

 

When I try to program the flash I get the message:

 

Beginning Operation...

____________________

Initializing remote connection...

Performing target initialization...

Error:   Connect Failed.

Can't connect. The Debugger can not connect to the P&E device (HC GDI Protocol Adapter)

Error:  command failed

 

Please, if anyone knows the remedy, please inform me.

 

The P&E USB Multilink Interface is about 2 years old.

 

Regards,

Jorgen

Labels (1)
0 Kudos
Reply
2 Replies

1,434 Views
jorgen2
Contributor I

Sorry everybody,

 

It was not a problem between Codewarrior and the BDM Multilink. It was an error on the target board.

 

In case anyone has a software add-on to CodeWarrior to troubleshoot the PC <-> BDM Multilink <-> target such that one can isolate the element with problems, please let me know.

 

I consider the case closed.

 

Regards,

Jorgen

0 Kudos
Reply

1,434 Views
ISUEE
Contributor I

Jorgen,

 

Could you give me a few more details of what your issue was/ how you solved it? I'm having a similar problem and could use any help/ advice. Thanks

 

EE

0 Kudos
Reply