Code Warrior 10 - failed connection to P&E USB Multilink Interface rev C

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Code Warrior 10 - failed connection to P&E USB Multilink Interface rev C

2,404件の閲覧回数
jorgen
Contributor I

I have installed the Code Warrior 10 on Windows 7 (32 bit). I have attached the P&E USB Multilink Interface Rev C to my PC and to the taget (an MC9S08SV16).

 

I have a program in C that compiles and builds without errors.

 

When I try to program the flash I get the message:

 

Beginning Operation...

____________________

Initializing remote connection...

Performing target initialization...

Error:   Connect Failed.

Can't connect. The Debugger can not connect to the P&E device (HC GDI Protocol Adapter)

Error:  command failed

 

Please, if anyone knows the remedy, please inform me.

 

The P&E USB Multilink Interface is about 2 years old.

 

Regards,

Jorgen

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,449件の閲覧回数
jorgen2
Contributor I

Sorry everybody,

 

It was not a problem between Codewarrior and the BDM Multilink. It was an error on the target board.

 

In case anyone has a software add-on to CodeWarrior to troubleshoot the PC <-> BDM Multilink <-> target such that one can isolate the element with problems, please let me know.

 

I consider the case closed.

 

Regards,

Jorgen

0 件の賞賛
返信

1,449件の閲覧回数
ISUEE
Contributor I

Jorgen,

 

Could you give me a few more details of what your issue was/ how you solved it? I'm having a similar problem and could use any help/ advice. Thanks

 

EE

0 件の賞賛
返信