CW8/DemoBoard56F8357/ProcessorExpert - Problem in Timer of bootloader

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW8/DemoBoard56F8357/ProcessorExpert - Problem in Timer of bootloader

2,218件の閲覧回数
howdeterminepwm
Contributor I
Hi all,
I have a problem in Bean FreeCntr one Time of example "demo_serial_bootloader". This example show the timer with parameter period of "1 second", i can't set this value in my project. The CodeWarrior show error message: "Timing settings failed in high speed mode - it is impossible to set the following items: initialization value."  about the value of timer. How i can set the one second in the bean? Can use other value to create bootloader in my project? peur example 139.000 mS, its ok? And the Prescaler? In example it's high:1 in my project i set "1", the IDE show "1" and show "High: not set" what's the problem? Thank u!


Message Edited by how determine pwm frequency on 2007-12-06 03:35 PM
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,006件の閲覧回数
trytohelp
NXP Employee
NXP Employee
Hi,
 
We should contact other department and probably Third Party to answer your request.
Can I suggest you to log it in the Freescale CRM system ?
Please use Freescale on line support web page.
  - Go to following URL: http://www.freescale.com/TechSupport
  - Click on Submit a Service Request. You will come to a login page.
  - You can submit your request through the web from there.
 
Pascal
0 件の賞賛
返信