CW8/DemoBoard56F8357/ProcessorExpert - Problem in Timer of bootloader

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CW8/DemoBoard56F8357/ProcessorExpert - Problem in Timer of bootloader

1,857 次查看
howdeterminepwm
Contributor I
Hi all,
I have a problem in Bean FreeCntr one Time of example "demo_serial_bootloader". This example show the timer with parameter period of "1 second", i can't set this value in my project. The CodeWarrior show error message: "Timing settings failed in high speed mode - it is impossible to set the following items: initialization value."  about the value of timer. How i can set the one second in the bean? Can use other value to create bootloader in my project? peur example 139.000 mS, its ok? And the Prescaler? In example it's high:1 in my project i set "1", the IDE show "1" and show "High: not set" what's the problem? Thank u!


Message Edited by how determine pwm frequency on 2007-12-06 03:35 PM
标签 (1)
标记 (1)
0 项奖励
回复
1 回复

645 次查看
trytohelp
NXP Employee
NXP Employee
Hi,
 
We should contact other department and probably Third Party to answer your request.
Can I suggest you to log it in the Freescale CRM system ?
Please use Freescale on line support web page.
  - Go to following URL: http://www.freescale.com/TechSupport
  - Click on Submit a Service Request. You will come to a login page.
  - You can submit your request through the web from there.
 
Pascal
0 项奖励
回复