CW10.1 code size info

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW10.1 code size info

ソリューションへジャンプ
2,372件の閲覧回数
Florijan
Contributor III

Hi,

 

I am new to CW10.1. Where can I get the info about the code size of my program and/or sub programs?

 

Best regards,

Florijan

ラベル(1)
0 件の賞賛
返信
1 解決策
1,806件の閲覧回数
CrasyCat
Specialist III

Hello

 

I would recommend you to take a look at the map file generated after linking.

 

If you are building code for Coldfire V1, look at the file with extension .xMAP generated in your build directory. 

You can see a section "# Memory map" in there which shows start address and size of each section inside of your application.

 

If you are building code for HCS08, look at the file with extension .map in your build directory

There is a section "SECTION-ALLOCATION SECTION", where you can see the size of each section defined inside of the application.

At the end of this section you can see a summary of the amount of memory used for code and constants (READ_ONLY), or data and stack (READ_WRITE).

 

The .map file generated by HCS08 linker also provide information of total amount of code, constant  and data in a section called "MODULE STATISTIC".

 

CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,806件の閲覧回数
Florijan
Contributor III

i am using Coldfire V1 and i will be using also s08 mcus.

 

best regards,

florijan

0 件の賞賛
返信
1,807件の閲覧回数
CrasyCat
Specialist III

Hello

 

I would recommend you to take a look at the map file generated after linking.

 

If you are building code for Coldfire V1, look at the file with extension .xMAP generated in your build directory. 

You can see a section "# Memory map" in there which shows start address and size of each section inside of your application.

 

If you are building code for HCS08, look at the file with extension .map in your build directory

There is a section "SECTION-ALLOCATION SECTION", where you can see the size of each section defined inside of the application.

At the end of this section you can see a summary of the amount of memory used for code and constants (READ_ONLY), or data and stack (READ_WRITE).

 

The .map file generated by HCS08 linker also provide information of total amount of code, constant  and data in a section called "MODULE STATISTIC".

 

CrasyCat

0 件の賞賛
返信
1,806件の閲覧回数
Florijan
Contributor III

Hi,

 

Thank you CrasyCat. Now i can see all the info about the code size.

 

Best regards,

Florijan

0 件の賞賛
返信
1,806件の閲覧回数
CrasyCat
Specialist III

Hello

 

Which MCU are you targeting (HC08, Coldfire, ...)?

 

CrasyCat

0 件の賞賛
返信