CW Windows

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW Windows

1,845 Views
bob_s
Contributor III

The CW environment is very helpful but there is one caveat I would like to see addressed.  I can have the Expressions window or the Target CPU window open along with code files, but those two do not show up in my pulldown windows select list.  If I want to see them on top I often have to shrink other open files to find them.   I think including them in the list would be a helpful improvement.

 

Thanks,

Bob

Labels (1)
0 Kudos
Reply
1 Reply

1,202 Views
J2MEJediMaster
Specialist I

You can always enter a service request, choose Technical Request and CodeWarrior on the service request web page, and then enter this as a feature request on the web page that follows. That way it will get reviewed by the engineers. There's no guarantee that they will implement the request, but at least it will be studied.

 

To enter a serivice request, click here.

 

---Tom

0 Kudos
Reply