Does Stand alone Flash Programmer tools support 56F803?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does Stand alone Flash Programmer tools support 56F803?

2,484件の閲覧回数
JeffZ
Contributor I

Hi everybody

 

I just found a stand alone Flash Programmer from freescale web. I downloaded it and tryed to flash 56F803. But I can not find configuration file from the itself file list. It seems it only support 56F8000 parts. is that true?

 

another question about this tools is: Does it support Macraigor Wiggler (parallel port)? When I tryed my Macraigor Wiggler, I got some errors.

 

JeffZ

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,309件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi,

 

The Flash programmer tool (56800E Flash Programmer.exe and fflash.exe) is not running for Hawk 1.

We recommend you to use the flash_over_jtag.

 

We've another version: flash_over_jtag.

Please refer in your installation under:

\ProcessorExpert\Tools\applications\flash_over_jtag\flash_jtag_loader_80x_82x

The tool is flash_over_jtag.exe. This is not a GUI.

Have a look to the doc: Flash_over_JTAG.pdf.

This tool doesn't support the USBTap interface.

You need to use a parallel cable plug on host and board.

 

It should work with the Macraigor Wiggler too.

 

Regards

Pascal

0 件の賞賛
返信