CW 8.2 debug

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW 8.2 debug

2,044件の閲覧回数
error3
Contributor I
Hi,

I'm using CW 8.2 with sincos demo board (MC56f8322). Everything's fine but it seems that i can't
see/check variables  (All) when the app is running, i can check their value only at breakpoints.
I'm new to this family, so is this normal ?? I'm used to HC(s)12 family and Cw 5.7 and there, I wasn't
expiriencing such issues, so..
Can someone help me on this?

Thnx for your replies.




ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,076件の閲覧回数
trytohelp
NXP Employee
NXP Employee
Hi,
 
If you mean a periodical refresh as the HC08/HC12, this is not available for DSC.
Under the Data menu there is Refresh Data.
This can be used.
Another option could be the Data Visualization tool.
Please refer to the Targeting_56800E.pdf, there is a chapter about that.
 
Hope this will help you
Pascal
0 件の賞賛
返信