CW 8.2 debug

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW 8.2 debug

2,055 Views
error3
Contributor I
Hi,

I'm using CW 8.2 with sincos demo board (MC56f8322). Everything's fine but it seems that i can't
see/check variables  (All) when the app is running, i can check their value only at breakpoints.
I'm new to this family, so is this normal ?? I'm used to HC(s)12 family and Cw 5.7 and there, I wasn't
expiriencing such issues, so..
Can someone help me on this?

Thnx for your replies.




Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,087 Views
trytohelp
NXP Employee
NXP Employee
Hi,
 
If you mean a periodical refresh as the HC08/HC12, this is not available for DSC.
Under the Data menu there is Refresh Data.
This can be used.
Another option could be the Data Visualization tool.
Please refer to the Targeting_56800E.pdf, there is a chapter about that.
 
Hope this will help you
Pascal
0 Kudos
Reply