CW 7.1 Debug problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW 7.1 Debug problem

2,470 Views
eric_prince
Contributor I

Hi team!

I'm using CodeWarrior 7.1 with a full licence.

My code compiles, but when I'm trying to open the Flash Programmer (by hitting Debug), IDEAuxiliaryResources.dll (v5.9.0, build 3024) pops a message saying: "Can't find executable file %s. It may need to be rebuilt.". Can you tell me under which circumstances (why!?) does this message come up?

Thanks!

Labels (1)
0 Kudos
Reply
3 Replies

2,270 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Eric,

Could you tell us which MCU  and operating system are you using?

Thanks in advance!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 Kudos
Reply

2,270 Views
eric_prince
Contributor I

After verification the target MCU is: MCF5234CVM150 (FREESCALE SEMICONDUCTOR : IC MCU 32-BIT COLDFIRE MCF5234 V2CORE 64KSRAM MAPBGA-256)

The operating system is Vista 32 bits.

Thanks for your patience. Can you look at the source code for that library?

0 Kudos
Reply

2,270 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Eric,

 

This CodeWarrior version has limited Windows Vista support, the latest classic version 7.2 does support Windows Vista 32-bit:

CodeWarrior® Development Tools for ColdFire®|NXP 

 

You will need to follow the TN268 in order to migrate to CodeWarrior 7..2:

https://www.nxp.com/docs/en/application-note/TN268.pdf 

Best Regards,

Carlos Mendoza
Technical Support Engineer

0 Kudos
Reply