Difference between Target Task and Run Configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Difference between Target Task and Run Configuration

1,496 次查看
francoisbronsar
Contributor I

Hello,

I'm running CodeWarrior 10.4 (Eclipse-based) and I have problems flashing a program to a board. Specifically, I can flash the program successfully if I select the project in the Code Warrior Projects view and use the Run As with the proper Run Configuration. That Run Configuration refers to a installation Task, say Install Program, to download the elf file generated in the compilation phase. If however, I select the Task Install Program directly in the Target Task window, with the same run configuration as above, and select  "Execute Task", the program is downloaded and installed but it doesn't start.  What is different?  I would expect that executing a Task with a given Run configuration would be equivalent as executing the Run Configuration with that task as the download step.  But it seems that it's not the case.  What is different and how do I use the Target Task to install and run the program?

Thanks,

François

0 项奖励
回复
1 回复

1,394 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello  François,

Could you please provide more information that I can reproduce your issue.

Which chip ?

Please take screenshot about your steps  when using RUN of  Target Tasks :

pastedImage_1.png

For simple , please first use the simple demo , for example LED .

BR

Alice

0 项奖励
回复