MPC5777C MCAL:ADC not support continuous mode without Interrupt

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPC5777C MCAL:ADC not support continuous mode without Interrupt

跳至解决方案
5,958 次查看
Ada_Lovelace
Contributor IV

Dear all,

I have a prolem, when I use the MCAL4_3 , I configurate the ADC,but It has the error.

When I choose the continuous mode and "without interrupt" mode, it has an error that:without interrupt feature is not supported for continuous conversion mode.

Do MPC5777C   must use interrupt mode about continuous mode? 

Or there is a problem about MCAL4_3?

pastedImage_1.png

标记 (3)
0 项奖励
回复
1 解答
5,528 次查看
Ada_Lovelace
Contributor IV

I have solved the problem.MCAL4_3  version has the bug , update the MCAL4_3  , ADC calibration makes it work.

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
5,529 次查看
Ada_Lovelace
Contributor IV

I have solved the problem.MCAL4_3  version has the bug , update the MCAL4_3  , ADC calibration makes it work.

 

0 项奖励
回复
5,872 次查看
mariuslucianand
NXP Employee
NXP Employee

Hello cuihan.ma@dotrustech.com‌,

In this community space, we are trying to answer questions related to AUTOSAR Application Layer generated directly from Matlab and Simulink. Please create a new thread on the MPC5xxx  space or new NXP support case according to the following procedure: https://community.nxp.com/docs/DOC-329745 

 

Hope this helps,

Marius

0 项奖励
回复