MPC5777C MCAL:ADC not support continuous mode without Interrupt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5777C MCAL:ADC not support continuous mode without Interrupt

ソリューションへジャンプ
5,743件の閲覧回数
Ada_Lovelace
Contributor IV

Dear all,

I have a prolem, when I use the MCAL4_3 , I configurate the ADC,but It has the error.

When I choose the continuous mode and "without interrupt" mode, it has an error that:without interrupt feature is not supported for continuous conversion mode.

Do MPC5777C   must use interrupt mode about continuous mode? 

Or there is a problem about MCAL4_3?

pastedImage_1.png

タグ(3)
0 件の賞賛
返信
1 解決策
5,313件の閲覧回数
Ada_Lovelace
Contributor IV

I have solved the problem.MCAL4_3  version has the bug , update the MCAL4_3  , ADC calibration makes it work.

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
5,314件の閲覧回数
Ada_Lovelace
Contributor IV

I have solved the problem.MCAL4_3  version has the bug , update the MCAL4_3  , ADC calibration makes it work.

 

0 件の賞賛
返信
5,657件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello cuihan.ma@dotrustech.com‌,

In this community space, we are trying to answer questions related to AUTOSAR Application Layer generated directly from Matlab and Simulink. Please create a new thread on the MPC5xxx  space or new NXP support case according to the following procedure: https://community.nxp.com/docs/DOC-329745 

 

Hope this helps,

Marius

0 件の賞賛
返信