zigbee broadcast to end devices

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

zigbee broadcast to end devices

2,584 次查看
AUAndrew
Contributor I
Hi,

I am not very familiar with the zigbee setup for networks.

I have a zigbee Personal Area Network with a coordinator and two end devices. I need to broadcast a message from the coordinator to the end devices that are connected to its network, but I don't know what I need to do to make this happen.

Any help would be greatly appreciated.
标签 (1)
0 项奖励
回复
3 回复数

1,058 次查看
Mads
Contributor V
Hi AuAndrew,
 
To send a broadcast to all devices you must use the 0xFFFF broadcast address.
If is ofcause also important that the ZigBee end devices must ofcause polling fast enough to recieve the broadcast.
 
BR,
Mads
 
 
0 项奖励
回复

1,058 次查看
neocronos
Contributor III
Where do I have to put 0xFFFF address? I tried replacing maDeviceShortAddress but it didn't work. When I have two devices, how does the coordinator decide which device will it send information to?

Thanks
0 项奖励
回复

1,058 次查看
neocronos
Contributor III
I could use a reply here, please?
0 项奖励
回复