zigbee broadcast to end devices

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

zigbee broadcast to end devices

3,392件の閲覧回数
AUAndrew
Contributor I
Hi,

I am not very familiar with the zigbee setup for networks.

I have a zigbee Personal Area Network with a coordinator and two end devices. I need to broadcast a message from the coordinator to the end devices that are connected to its network, but I don't know what I need to do to make this happen.

Any help would be greatly appreciated.
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,866件の閲覧回数
Mads
Contributor V
Hi AuAndrew,
 
To send a broadcast to all devices you must use the 0xFFFF broadcast address.
If is ofcause also important that the ZigBee end devices must ofcause polling fast enough to recieve the broadcast.
 
BR,
Mads
 
 
0 件の賞賛
返信

1,866件の閲覧回数
neocronos
Contributor III
Where do I have to put 0xFFFF address? I tried replacing maDeviceShortAddress but it didn't work. When I have two devices, how does the coordinator decide which device will it send information to?

Thanks
0 件の賞賛
返信

1,866件の閲覧回数
neocronos
Contributor III
I could use a reply here, please?
0 件の賞賛
返信