trouble programming 908jk3 with cw5 and usbmultilink

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

trouble programming 908jk3 with cw5 and usbmultilink

1,523 Views
eeetee
Contributor I
hi:
 
i'm missing something very elementry i'm sure! the code is very simple and disassembles as expected. the programming script runs with no errors. of note, when i go to the memory window and check the reset vector the entire ec00 to ffff shows "rr" for data. if i go to the assembly window it shows the code as written. if i click on the right hand scroll bar the code changes to seemingly random code. the programer is functional as i have programmed some qt4 devices with no problem. what am i doing wrong?
 
thanks in advance
 
 
ed taylor
 
; export symbols
           XDEF _Startup, main
           INCLUDE derivative.inc
;            INCLUDE MC68HC908JK3.inc ;     'derivative.inc'
           INCLUDE ed.inc
; variable/data section
;MY_ZEROPAGE: SECTION  SHORT         ; Insert here your data definition
 
           
RAMStart    EQU  $0080  ; absolute address to place my variables
           ORG   RAMStart
variable1:  RMB 1
 
           ORG   ROMStart
           
; code section
main:
_Startup:   rsp
;hardware init
           mov   #%11111111, DDRA      ;porta is not bonded set as outputs
           mov   #%00001100, DDRB      ;portb d7..d4 analog, d3=redled d2 grnled, d1,d0 mono8 interface
           mov   #%00110011, DDRD      ;portd d7,d6 undefined digital inputs, d5,d4 injector drv, d3,d2 analog current monitors d1,d0 unbonded
           
 ;           bset  3,PTB
 ;          bset  5,PTD
  ;         bset  4,PTD
           LDA   #%00001100
           sta   PTB
           bra *
;            CLI                     ; enable interrupts
mainLoop:
           ; Insert your code here
           NOP
;            feed_watchdog
           BRA    mainLoop
 
;**************************************************************
;*                 Interrupt Vectors                          *
;**************************************************************
 ;            org    $FFDE         ;beginning of QY4/QT4 vectors
;VADC:        fdb    spurious        ;point to alternate vectors
;VKBD:        fdb    spurious
;* There is a gap from $FFE2-FFF1 that is used for user monitor code
            org    $FFF2         ;skip unused vector locations
;VTOF:        fdb    spurious
;VTCH1:       fdb    t1_isr
;VTCH0:       fdb    t0_isr 
;             fdb    $FFFF         ;fill unused location with $FFFF
;VIRQ:        fdb    spurious
;VSWI:        fdb    spurious       ;SWI service routine in Mon08 ROM
             org   $FFFE
VRESET:      fdb    main      ;to start of user code

END
Labels (1)
0 Kudos
Reply
1 Reply

734 Views
eeetee
Contributor I
hi again:
 
i'm feeling a little dumb right now. i had been playing with the linker files and didn't restore them correctly. that combined with a bad solder connection and a failed led took me on quite a chase. all is well, i just didn't know it.
 
 
regards,
 
ed
0 Kudos
Reply