programmable pins of MC68HC908QB8

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

programmable pins of MC68HC908QB8

3,110 次查看
abhi_roy03
Contributor I
Hello
I am using MC68HC908QB8 microcontroller in my project.Can i connect port A of the microcontroller to the programmer.The microcontroller has 16 pins in total.It has 6 pins which are dedicated for multiple purposes(I/O port,A/D channel,Key board interface bits).if notkindly update me on the programmable pins of the QB8 microcontroller.
 
regards
Abhishek
标签 (1)
0 项奖励
回复
2 回复数

785 次查看
RaghuSorab
Contributor I

Hi Abhishek,

To the best of my knowledge, all the QT Devices have the PTA0 as the COM, PTA4 is tied to ground and PTA1 is tied to VCC.

It is the MON08 standard. Please do refer the programmer manual in which the MON08 pinouts for the specific Device will be given.

Hope this makes it clear.

Raghu Sorab

 

 

 

0 项奖励
回复

785 次查看
peg
Senior Contributor IV

Hi Abhishek,

I am not sure what you are asking...

The MON08 pins of this device are all on Port A already.

All MON08 functions are tied to a particular pin, you cannot change this!

Maybe try to rephrase your enquiry.

Regards David

 

0 项奖励
回复